I recently purchased the Seeed EdgeBox RPI4 and am trying to set up with WM1302 SPI LoRa module. There are no instructions or settings in the Seeed EdgeBox RPI4 documentation so am using LoRaWAN® Gateway Module WM1302 - Seeed Wiki (this uses a Pi hat to connect to WM1302) but am getting error when running ./lora_pkt_fwd -c global_conf.json.sx1250.US915 command. Error happens when opening SPI communications interface per below:
CoreCell reset through GPIO17…
SX1261 reset through GPIO17…
CoreCell power enable through GPIO18…
CoreCell ADC reset through GPIO13…
Opening SPI communication interface
ERROR: [main] failed to start the concentrator
Can you verify what pins should be set in reset_lgw.sh script ?
Thank you,