DSOQuadV2.6 RESOURCE(Update 2012/04/12)

Now the .hex can be installed on my DSO, but I get the same result as when I compiled your v1.0 myself: 1/2 of the time a black screen, 1/2 of the time half a second of parasites, then a freeze.

I use SYS150_1.6 (from marcosin 1.8). No idea about the FPGA, but I bought my DSO about one month ago, so I guess it should be the latest.

Marco’s firmware works well, so the problem has nothing to do with the source code. Gabonator’s port of the firmware (valky.eu/data/hardware/ds203 … soquad.zip) compiles and works well too with the same toolchain as Pedro’s, so it seems it’s not the toolachain… so what?!?

Unfortunately, my debugging opportunites are inexistent and I have not the slightest knowledge about the used tools… and thus no hope of installing Pedros’s modifications or improving myself Marco’s firwmare!!!

This is very frustrating…

Patrick