I tried both 4 and 3 slot programs on my HW V2.81 with no problems. I’m also running SYS version 1.62 which was installed on the device when it was shipped from the factory.
Was thinking if he loaded the 3 slot first, that might somehow free up his corrupted device for subsequently reloading your 4 slot (larger) program. If that works and he still can’t safely reformat his 8GB flash drive due to connectivity problems, then he must have a corrupted operating system or older version than SYS version 1.62.
Your HW 2.72 has 8GB flash drive too, same as HW 2.81.