DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)


That’s strange. The code for both versions is exactly the same, save for a couple of lines I removed in the 3 slot version,

which I can’t imagine could cause any problems.

The larger version maps the program to a different part of the ROM, but to the same place as V4.3, it just has a bit more

code at the end, but well short of the V2.81 FPGA.



I just downloaded the post and loaded the main hex to one of my devices just to make sure , and everything worked OK.

However, all of my devices are HW 2.72.



Borland, you stated you loaded the program on your V2.81 device with no problems, did you try to load the main

version, or just the 3 slot version as you suggested?



Has anyone else successfully loaded the main version on HW2.81? I double checked the memory mapping, and can’t

imagine any reason it would not work. Perhaps a corrupted file?