DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)

First off, thanks to pmos and all the devs that have turned the Quad into something much more than when I first got it a year and a half ago.



I was wondering if it would be possible get multiple binaries for this community edition, packaged for alternate slots? With several great firmwares available, it would be nice to be able organize them into different slots without having to reflash to run a different firmware.



I built a hex 1.29 locally compiled for slot two, but it crashes (freezes at loadup screen and beeps constantly). The binary I downloaded for 1.29 run’s fine(in slot one). I used the 2013q1 arm-eabi-none toolchain from Launchpad, but I manually “installed”(unzipped) it to a temp folder and hacked up the built script and environment to avoid interfering with some other gcc toolchains I have installed. So it’s entirely possible I goofed it up somewhere. From reading some of the other forums, I’m a little worried I’m going to hose my bootloader with a bad build.



Thanks again,



Jon