order
March 9, 2013, 8:27am
221
Ok, before power cycle, I can do a umount/mount cycle, and check of the upgrade result:
SYS25116.hex -> SYS25116. RDY
APP_G251.hex -> APP_G251. RDY
CFG_FPGA.ADR -> CFG_FPGA. ERR
Dunno, should I proceed with V261FPGA.BIN too?
Why the error?
Ok, I proceeded:
V261FPGA.BIN -> V261FPGA. NOT
Any hint?
Some more tries:
downloaded FPGA_v222:
http://garden.seeedstudio.com/images/2/23/FPGA_V222.rar
CFG_FPGA.ADR -> CFG_FPGA. SET
V222FPGA.BIN -> V222FPGA. NOT
downloaded FPGA_V25:
http://garden.seeedstudio.com/images/1/12/FPGA_V25.rar
CFG_FPGA.ADR -> CFG_FPGA. SET
FPGA_V25.BIN -> FPGA_V25. NOT
Ok, I really stuck.
Maybe the firmware upgrade is too old?
I see this:
[code]
DSO QUAD
Device Firmware Upgrade V3.10
Please copy .Hex/.Bin file to
DFU virtual USB disk.
[/code]
Best,
Laszlo
order
March 9, 2013, 9:26am
222
Reading the wiki one more time, I got the idea, what if I reupload an older sys, app, fpga firmwares in that order, and maybe the fpga down the line success.
So, downloaded:
http://garden.seeedstudio.com/images/c/c4/SYS_B134.rar
http://garden.seeedstudio.com/images/f/f9/APP_B232.rar
http://garden.seeedstudio.com/images/2/23/FPGA_V222.rar
And uploaded to the devices, one by one:
SYS_B134.hex -> SYS_B134.RDY
APP_B232.hex -> APP_B232.RDY
CFG_FPGA.ADR -> CFG_FPGA.SET
V222FPGA.BIN -> V222FPGA. NOT
Also tried these too:
Sys_151: <LINK_TEXT text=“http://www.seeedstudio.com/forum/downlo … php?id=857”>http://www.seeedstudio.com/forum/download/file.php?id=857 </LINK_TEXT>
App_252: <LINK_TEXT text=“http://www.seeedstudio.com/forum/downlo … php?id=856”>http://www.seeedstudio.com/forum/download/file.php?id=856 </LINK_TEXT>
FPGA261: <LINK_TEXT text=“http://www.seeedstudio.com/forum/downlo … php?id=858”>http://www.seeedstudio.com/forum/download/file.php?id=858 </LINK_TEXT>
SYS_B151.hex -> SYS_B151.RDY
AP1_B252.hex -> AP1_B252.RDY
CFG_FPGA.ADR -> CFG_FPGA.SET
V261FPGA.BIN -> V261FPGA. NOT
Still no luck. Any more ideas?
Best,
Laszlo
Bravo to the authors for the great work.
When can we expect a new version.
Regards, Peter!
pmos69
April 8, 2013, 12:05pm
224
Available time has been quite rare, so I can’t really say.
I have a few things in the development ToDo, but haven’t been able to get anything done.
(unless more code contributions come in, and in that case I’ll have to find the time)
This DSO203 GCC APP works with hardware 2.7 ?
pmos69, thanks for the great work and fast response.
If I can give some suggestions:
Is it possible to start by changing the color of the testimony in FFT mode from red to yellow or green. Red is fuzzy.
To add to the ranges of horizontal scanning 50nS/del.
Automatic switching between the range of the horizontal sweep.
As with Chip’s APP.
Regards !
Peter
HW: 2.70, Sys: 1.52, GCC App: 2.51 (http://pmos69.net/dso203/APP_G251.hex ).
Bug: actual generator frequency is 2 times lower than selected in all modes except PWM.
I have downloaded: https://github.com/pmos69/dso203_gcc/zipball/master
compiled, updated firmware. DSO shows initial screen with version and hangs.
I noticed that http://pmos69.net/dso203/APP_G251.hex is not compiled from this source.
What is wrong?
My toolchain version:
arm-none-eabi-gcc (GNU Tools for ARM Embedded Processors) 4.7.3 20130312 (release) [ARM/embedded-4_7-branch revision 196615]
GNU assembler (GNU Tools for ARM Embedded Processors) 2.22.0.20130312
You are absolutely right counterpart. Software is great, but I want some finishing and supplements.
Also not working properly vertical scanning ranges of volts / div.
I think you have the wrong sys file loaded to get that bug. Check OP and use the linked sys25116
Hello,
I want to ask some of the authors of the software to show me where exactly are configured ranges Horizontal scanning: 1S …0,1uS.
The idea is to add a range of 0.05uS.
Thanks in advance!
P.S: Time for v1.30!
First off, thanks to pmos and all the devs that have turned the Quad into something much more than when I first got it a year and a half ago.
I was wondering if it would be possible get multiple binaries for this community edition, packaged for alternate slots? With several great firmwares available, it would be nice to be able organize them into different slots without having to reflash to run a different firmware.
I built a hex 1.29 locally compiled for slot two, but it crashes (freezes at loadup screen and beeps constantly). The binary I downloaded for 1.29 run’s fine(in slot one). I used the 2013q1 arm-eabi-none toolchain from Launchpad, but I manually “installed”(unzipped) it to a temp folder and hacked up the built script and environment to avoid interfering with some other gcc toolchains I have installed. So it’s entirely possible I goofed it up somewhere. From reading some of the other forums, I’m a little worried I’m going to hose my bootloader with a bad build.
Thanks again,
Jon
Can anyone publish a “C” code SYS25116, because I find only HEX file.
Thanks in advance!
pmos69
April 22, 2013, 1:07pm
235
Here’s the source code for Marco Sinati’s SYS25116.
Be aware that it wasn’t made for compiling with GCC.
pmos69
On line 137 of Menu.c an error instead:
{(char *) CH_D_STR, (u16 *) Y_INV +3, 14-1, CIRC, 188, 228, 1, UPDAT}, / / Track sourtse
should be:
{(char *) CH_D_STR, (u16 *) Y_INV +3, 15-1, CIRC, 188, 228 1, UPDAT}, / / Track sourtse
to exit a menu: SPEC_B.
If you have the time and opportunity point me where to look for ranges of horizontal scanning 1S … 0.1 uS. The idea is to add a range of 0.05uS and automatic switching between the range of the horizontal sweep.
I would like to get involved in improving the software.
Thanks in advance!
I can not add files in the forum!!!
Publish one of my version of the software, without claim to any copyrights, because I have not changed anything substantial changes:
Removed bug for displaying SPEC_B.
Changed the colors of the FFT, I do not know whether the most appropriate, but I personally do not red fuzzy.
In Trig menu is added FulAU which currently doubles AUTO menu, but the idea is to osushtestvi automatically switching range of the horizontal sweep.
If you like, use it!
P.S: Use with: SYS25116
[size=150] I want to emphasize that this is v1, 29, Pedro Simoes whit small cosmetic changes![/size]
I have two questions to [size=150] pmos69[/size]:
SYS1.6, who publish the same as it is SYS25116.
With what compiler to work after changes in the SYS file.
I apologize in advance that you are wasting time and Thanks!