tgo,
Just a thought, the current source code (APP_235, SYS_134) is not particularly complex, or well written for that matter (chuckle). It would be not so difficult to simply write these again in a similar way that BenF has done with the Nano. BenF’s APP_313 appears well coded and well structured, as professional software development should be.
Now it would be great not to have to re-invent the wheel for the Quad DSO since BenF has already progressed so far with the Nano. Looking through the APP_313 source, there are many, many coding structures that could simply be ported directly to the Quad DSO, and then built upon in order to suit the Quad DSO. The other nice thing with this is that there would be consistent features and usability between the Nano and the Quad DSO.
So I would ask, how about it BenF? Are you prepared to share the source code for v3.62 under the basis that it is to be ported to the Quad DSO and then developed to work with that hardware, by those people that would like to take it on?
The comment that the Quad DSO is a “diamond in the rough” I feel is correct about the Quad DSO, and after looking at the hardware design and currently available resources, it has a lot of potential but is not there yet .