DSO Quad suggestion and bugs.

Lygra … Am i missing a trick here … is there an SD card on the quad, what size and where does it go.

One of the reasons that BenF gave for not being able to save large export files was due to the limited size of the internal memory AKA flash drive. If this can be made larger or better still an exposed SD card slot we could actually have several sets of configs made portable on the SD cards. I can see me with a library of saved waveforms and settings on different SD cards.

CHeers Pete.