DSO Quad suggestion and bugs.

It’d be great if in new release will be this things and fixed buges:

  1. realtime drawing of ray(as on analog scope) :exclamation:
  2. correct voltage measurment
  3. correct FRQ measurement unit(Khz,Mhz istead of Hz) :wink:
  4. higher speed of moving cursor(xpos), depending on wheel button pressing time
  5. smooth adjusment of signal generator, at least wave generator(!!) + wider range of generation
  6. visual selecting not only submenu, but and menu(crossing, shadowing, color changing…)
  7. the worth, dat/buf file loaded from memory don’t scrolling(xpos) :exclamation:
  8. in single mode 5,10,20,50,100uS doesnt work

As for hardware, there two problems:

  1. bad digital probe, one loosing contact near the connector, and both very hardly getting out from oscope
  2. terribly jog wheels!!! the upper end is too short, pressing it is uncomfortable.

Btw, is there any program on pc to watching dat/buf files?

PS My device is 1.50sys 2.50(or 2.52, in screen it says 2.50, but i firmwared it 2.52…)app