DSO Quad suggestion and bugs.

Hi there,

I’ve notices some bug now… some of them are already on the forum some don’t (?)

When using the single shot mode… It would be very handy if it where possible to alter the XPOS especially when the span of the signal exceeds the screen.

I also have troubles with the calibration of the quad. The ground level is wrong after the calibration procedure… as is the VDC level… It’s never correct.
The procedure I did by the book… and as a reference multimeter a fluke 289…

To my opinion the UI isn’t handy at all… not quite structured and way to much jog switch actions involved. I really would like some interface with the same intuitive interface as for example the benf 3.62 on the nano…

When changing the V/div parameter the GND offset changes along staying at the same relative error.

sometimes the thing locks up on me… Mostly this is when i’m tinkering with the time/div and the triggering mode. Not jet discovered the exact cause.

suggestions:
It would be nice to have:
Signal generator with control of the duty cycle.
A logging style function (like the fluke trend-view) which would preferably store to the internal memory.
A life link to the PC using the USB, so a choice whether to show as USB drive or as for example a com port.
When using 100 ms + Time division It would be nice to know how far the 4096 sample buffer is filled up.
using the wave out… A signal tracing feature…
Multimeter style display Just show (auto ranging) the voltages on the two analog inputs.

Best Regards,

Matijs

Found an other bug:
When saving to CSV, BUF or DAT after a single shot trigger… The file stays empty…
When trying to open this file with the QUAD it crashes (later on i figured the file is empty/0 bytes)