DSO Quad Logic analyzer application

Great! Nice to see that somebody is still working on the DSO Quad.



I agree with Johan, the thing I miss most are the timescale display and some cursors.



Congratulations!



Two questions to the author:



How can I download the source code using Windows (without having to download each file separately)



Regarding your superb frequency response analyser: i’m trying to extend the range up to 2MHz, and I try to use the “set_square_frequency” function for generating frequences above 200kHz. But the DSO crashes (hangs) when I call this function. The ___Set (DIGTAL…) calls are the cause, even with good parameters, but I have no idea why!



Patrick