Sounds interesting; I don’t have any experience in designing SMPS, though.
The DSO Quad analog inputs have some protection already built-in, so the separate buffer may not be strictly necessary.
If you are ok with rebuilding from source (should be quite easy, following the instructions in README), you can adjust the dB scale in the source code. It is in main.c, “MAX_DB”. Default value is 10, just increase it (and also MIN_DB if you want).