DSO Nano v2 issues and FAQ

[Space for Frequently Asked Questions]



How to save waveform and configuration into SD card :



1 . Make sure your SDcard supports SPI mode. (Most SDHC and over 2GB card does not)

2 . Format your SDcard with FAT16

3 . Create a new file named FILEXXX.DAT in your SDcard root (file size must bigger than 1KB). Or directly download here and copy it into SD card root.
[attachment=0]SDFILE (1).rar[/attachment]
4 . To save the waveform : move the cursor to FS option, choose the file you want to save , then press “OK” .



Is the X10 and the X1 use the same Probes

No , if you want to use the X10 , you have to use the X10 probes .



Is DSO Open source ?

The F/W (APP) will be open source and all people can use or modify them freely, but there is some third party code included in LIB and we don’t have the authorization to publish them.



The H/W is open source for all version.



Why can’t i compile the project code

The source code was built by IAR 4.2, IAR 5.x is not supported.
SDFILE (1).rar (4.84 KB)