Yes, you are right, totally. But I did not want to make my post longer so I waited for somebody to solve this problem. Of course I miss a x10 probe now, maybe with a little switch x1/x10. And of course there is a need for input protection. Sorry for misunderstanding: I did not want to create another multimeter or an oscilloscope for high voltage. My proposal is, to improve and simplify one of the most used functions in daily life (voltage in numbers and shape). This function is already implemented now, but - at the first glance - hidden very well under a lot of lines, colors and options.
My proposal is inspired by the small format of the NANO: when working on your table you can use a larger instrument with larger bandwith etc. But working outside with a pocket size instrument often means working under pressure and in poor conditions, and you will be glad to see just the most important without need of make settings.
I think, the topic is “how to improve the NANO” and that’s just a proposal. It was born by the fact that the NANO would not lie on my table in order to explain it to an employee if it wasn’t a little bit complicated.