BenF,
I’m sorry (and somewhat embarrassed) to just keep throwing out requests … I’m new to this wonderful device, and if nothing else, I want to document my wish list as I run across issues using it.
I’m looking at some serial data packets with relatively long delays between packets. When I try to zoom in on an area, it re-triggers on other bits in the same packet making things look a bit unstable. It appears there is no way to force a standard trigger hold-off so that it will wait until the first bit of the next packet?
Again, this is not ultra important. I realize its easy for me to request new features, while you are the one that has to triage all the requests (by the looks of it, some pretty crazy ) and do the real work of implementing them. I can’t imagine how much time you spend on this. Anyways, if nothing else, add it to the list for some day when you have too much time on your hands … ha ha
.
Thanks again,
Dave
P.S. An after thought … it may be triggering in the middle of a subsequent packet rather than re-triggering within the same packet. Not sure how that timing in the code all works out? In any event, it would be useful to add (additional) trigger delay to push it out to the start of a new packet.