DSO firmware version 3.64

Benf,

Just few additional comments and ideas.

We need Average, Min and Max values per each t. You can use Average values as replacement for you old samples: for displaying waveform, triggers, saving, … The Min and Max can be used only for displaying high freq components with lower color intensity.

The nature of Average value is actually Low Pass filter, which is good and eliminates high freq noises. The Min and Max displays these high freq values. With current values we have these mixed and cannot see any of them on best way.

My idea for calculating Avg is simplest possible, and it is better then nothing. Theoretically, it is possible to make more quality Low pass filter (for this re sampling purpose) using formula c0v0 + c1v2 + c2v3 + … + cn vn, but this require memory for storing ci. I suggest to use my simplest possible approach suggestion.

Another ideas: in Normal and Single sync modes, we cannot see the signal until it is catched. It is possible to display always current signal changes, while triggered signal (and hold signal) could be displays with another color, for example red (actually light red for Avg value, and dark red for Min/Max). On this way we adjust trigger position and see signal while we are waiting on catching trigger.

The trigger mode is important option, so it has a sense to be separate menu, similar as TD, VD.

The Auto mode can be spitted in on two modes. Old Auto and new Auto which display new waveform immediately if trigger is not cached. It can be used in Normal and Single mode too for current “green” signal while holding signal is red.

Some links:
en.wikipedia.org/wiki/Circular_buffer
en.wikipedia.org/wiki/Xiaolin_Wu … _algorithm
en.wikipedia.org/wiki/Downsampling

Thanks,
Dejan