DSO firmware version 3.64

BenF;

  1. In your Firmware User’s Guide, on page 13, you describe a calibration procedure using a DC voltage. Is it possible to establish gain calibration using a different procedure that would support the use of a function generator AC signal to establish gain calibration?

The reason I ask is because many more users have function generators than variable DC voltage supplies. If we use an external calibrated o’scope to measure the input waveform amplitude, could we use something like Vpp?

  1. In the Measurement section of your Firmware User’s Guide, on page 11, you discuss the measurement of an AC signal. When you refer to the number of complete acquired waveforms, are you referring to the capture buffer or the display buffer as the source for these acquired and measured waveforms?

Thanks