DSO firmware version 3.64

Vow! - That was quite a list of ideas and implementation details on your part.

Perhaps you could single in on your most desired enhancement and present a simple use case / example that I and others can comment on where you focus on the actual measurement and desired result rather than the implementation?

One of your ideas is to always sample at 1Mhz (the Nano maximum sample rate) for all T/Div’s. When we sample at 1MHz, time between 1st and last sample (for one capture cycle of 4098 points) is approximately 4ms. For a T/Div of 10ms, all we would see plotted then is a tiny waveform about 12 pixels wide. Surely this is not practical and so a compromise is needed.

Another idea of yours is to capture two points per on-screen pixel as opposed to one. With the current firmware and using fast buffer mode we capture 10 points per single pixel.

Visual perception is also an aspect to consider. Current refresh rate is 10Hz (300 points redrawn 10 times every second) and this is about as much as we humans can comprehend. If we increase refresh rate further, consecutive capture cycles will appear as if they blend together. If we need to capture a specific waveform detail we may be better off letting the DSO do the hard work (continues sampling) and then stop and show us (trigger) if and when an issue is found.

You’re also suggesting there are issues with using fast buffer mode and Normal trigger. Perhaps you could expand on this with some examples?