DSO firmware version 3.64

Hi BenF,

I was thinking more about my suggestions, and have another ideas.

Related to capturing always on higher possible frequency and MIN and MAX values, when I better think, it is better to capture three values:

  1. Averatage Value – used to draw lines as you did before
  2. Min value (apsolute difference of average value)
  3. Max value (apsolute diffrence of average value)

To be able to save buffer memory, the normal average value can be stored with 8 bit, while DIFFERENCE of average value to Min and Max can be stored with 4 bit resolution per each (2x4 = 8 bit).

Because these 4 bit is very low resolution (only 16 values), and because these min and max will be usualy close to Average, the none linear converion is needed: Smaler distance need to be stored with bigger precision then other. For example, the table like this:
Diff Min/Max Value Diff stored in buffer


0 0
1 1
2 2
3 4
… …
7 7
8 8

< 10=8+2 8+1=9
< 12=8+4 8+2=10
< 16=8+8 8+3=11
< 24=8+16 8+4=12
< 40=8+32 8+5=13
< 72=8+64 8+6=14

= 136=8+128 8+7=15

There could be better non liner functions, but I guess this is simple to realize.

To simplify proggramimg, you can draw your lines as you alredy did, but before you draw line, the program displays the vertical line between min and max value with lower intesity color. There are other possibilitis to draw and fill lines between Mins and between Maxs with better look, but that is not important.


For auto option, if trigger is not found, while to wait 100ms for new display. Let’s display this as soon as possible, ot better, give the user posibilty to define that time.


If you need to extends your user interface with more options where some of them requires entering values (for previous option, fs for filters, …), I suggert to make routine for entring these numbers. I’ve put the picture what I’m using on my application which uses only 4 keys for user interface (Up/Down, Esc, Ok).


This option is not important and it is hard to implement, but it gives great look. If neded, it is possible to diplay full input resulution on smaler screen resolution using antialiasing lines which uses differnt color intesity. If somthing is between two pixels, but it more close to one, you can display an value with highr color intesity then on another. But the sum intesiy of all pixel need to be the same. Example from UBUNTU screen.

Regards,
Dejan