benf- if there was one thing to make this product better–>i vote again for option to eliminate buffer in 1m/s- 50m/s division that would be very useful for automotive techs like myself as the expensive scopes have such a slow screen update rate in the 1m/s range, i would use this option and the buffer that currently exists to get the info i need from the diagnostic situations that i get into, its like the best of both worlds(resolution of the current buffer and the speed of the elimination of buffer option to see the fast trends that occur)