DSO firmware version 3.52

Dear BenF,

Great work. I got myself a DSO Nano v2 today and the first thing I did was to load your firmware onto it. Much nicer without all the garbage dots on the screen and nice pop-up menus.

Just wanted to ask whether we can get logging to SD card working? Even if the sample rate is only say 100Hz, I would love to be able to say log the voltage across a battery running down over half an hour. Would make a very nifty hand-held pocket sampler. Would be great if you could say add different sample rates, and or a timed-logging function. If to save processing power and SD-card bus speed limitations, I don’t mind if it’s raw PCM or what - just something we can post-process on a computer. I think that would truly get me off my old cheap USB Oscilloscope units that are always crashing my PC!

  • Gough