No one can really check if he has written the version from scratch because it is still unreleased (he says he did, but that is only his word). One think you can check is the fact that he uses his own copyright (it is displayed all over when you start up). Probably he also put his copyright on a lot of Seed’s open source work which isn’t very nice to begin with.