When is connected to PC via USB, then on DSO’s disk are visible files in moment of connection. When are saved f.eg. screenshots, on disk are visible after unplug/plug.
Why ?
When is connected to PC via USB, then on DSO’s disk are visible files in moment of connection. When are saved f.eg. screenshots, on disk are visible after unplug/plug.
Why ?
If you are using Windows then I find like you that the new file written by DSO does not trigger a refresh.
Pressing F5 to force a local refresh doesn’t seem to help, but I find that if I close Windows Explorer completely and re-open it then that does force a full refresh and new files show up. Slightly tedious but probably easier than re-connecting the USB.
The file write by the DSO is working but something is not triggering the ‘file changed’ event.
No, it does not work on my W8.1.
I am DSO newbie ( versions 2.81/1.62/1.13)
I am using Win 7 Pro. It is quite possible the Explorer cache works differently on 8.1
I did do a check using a low level partition tool and saw that a new file written by the DSO turned up there.