Hi,
I’ve bought the DSO203 from Amazon. I installed Gabonator’s app on slot 1 and the pawn framework on slot 4. I then wanted to install some pawn-scripts, but couldn’t, because the USB storage didn’t show up in Windows. Before that, I tried to same a bmp from Gabonaor’s UI, when I restarted, the settings where all gone and the app crashed, because with “assertion failed”. I think the saving process overwrote the settings somehow…
Now I can’t get it to work correctly. When I flash the latest FPGA and SYS_B1.60.hex, I can’t save settings and when I mount the USB Storage on linux, it only has some weird files like with unsopported chars (�) on it, which state to be several GBs big. I also can’t write on it, because it is read only.
My hardware version is 2.72. At least that’s what is printed onto the pcb, but the amazon description states 2MB, which would point to an older version.
How can I get it to work?
My goal is Gabonator’s app on Slot 1, the community version on slot 2, and the pawn-part on slot 4.
Thanks in advance,
Benedikt