Hi There!
I was using my DSO203 for a while with Wildcat6.5 without problems.
I was reading about upgrading the FPGA to get full speed oversampling, “copy FPGA_281.ADR then FPGA_281.BIN in DFU mode to the device”, so I thought to give a try.
Now my DSO displays “FPGA configuration error please load the FPGA data” then on the next screen a color dotted rectangle (it looks like the logo is missing) and below it shows “Hardware Ver 2.82 Serial No:” (Serial no is empty) and keeps peeping continuously.
[attachment=1]IMG_2435.jpg[/attachment]
In DFU mode Serial and Licence is displayed correctly.
[attachment=2]IMG_2436.jpg[/attachment]
My device is DS203 HW2.82 DFU V3.46C
Can someone give me some instructions to get my device working?