After installing DfuSe_Demo_3.0 and connecting my DSO nano to the PC
Windows7/64 searches for the driver but cannot find it.
What did i wrong?
(Current DSO Nano firmware is V1.520 and i liked to upgrade it to V2.4)
Tolle
After installing DfuSe_Demo_3.0 and connecting my DSO nano to the PC
Windows7/64 searches for the driver but cannot find it.
What did i wrong?
(Current DSO Nano firmware is V1.520 and i liked to upgrade it to V2.4)
Tolle
In addition:
In Windows7/64 / manager / usb-controller the DSO Nano appears as unknown device
(Code 43).
The Dso nano is installed with the dfu’Se Demo V23.01 Setup_x64
tolle
Correction:
DfuSe V3.01 Setup x64
tolle
Problem solved.
For driver installation the starting sequence of the dso nano is to hold the M- Button when starting.
The rest is as described.
tolle