Windows select the silicon Lab driver directly, I don’t understand why it doesn’t take that of the st.
Anyway yes, I can connect through a terminal and send AT commands.
The problem is when I want to program the card with my code
I cannot connect via STM32CubeProgrammer, if i try to connect via st-link, the program doesn’t see anything, same with usb. With UART, it tries to connect but fails.
I tried to force the stm driver but nothing changes