Good day to all.
I’m trying to get BenF’s new 3.62 firmware into my DSOnano v1 but am having problems getting DfUse 3.0 to run.
This is a relatively new netbook (i7 quad-core) running Windows 7 64-bit. I’ve previously used this version on my older netbook running Windows XP 32-bit.
The symptoms are: I get a UAC prompt asking me to approve DfUse, then I see the usual ‘wait’ hourglass for a few seconds, then nothing.
Opening the Windows Task Manager shows that at least 3 processes are started when I launch DfUse: 2 of DllHost and one of DfUseDemo. The two instances of DllHost disappear fairly quickly, one after the other, then DfUseDemo goes away after another 10 - 15 seconds.
I’ve played with the compatibility options but nothing has helped so far.
FWIW - the other two apps bundled with DfUse both run correctly: stdfu Tester and dfu file manager. But they aren’t what I need.
Is there a newer version of DfUse available that is rated for use with 64-bit Windows 7?
Many thanks!
dwayne