Hello, i ordered a grove O2 sensor and im making a 3D printed housing for it. i was searching the web for the dimensions of the pcb. but couldnt find anything.
Can someone measure this for me?
Greetings
Hope this helps @Mathias_Vangompel
A= 40mm
B= 20mm
C= 30mm
D= 10mm
All dimensions are to the center of each hole
Hole dimension is 3mm
Note :- Each hole is on the edge of the board and the board can not lie flat, there is the connector terminal one side and circuits the other so it needs a stand off on each mount.
Please see additional photos for clarity.
Hi, you also can download eagle board files from <LINK_TEXT text=“https://github.com/SeeedDocument/Grove_ … ics_O2.zip”>https://github.com/SeeedDocument/Grove_Gas_Sensor_O2/raw/master/resources/Schematics_O2.zip</LINK_TEXT>. then click Draw–> Dimension to measure the sizes. thanks.
Seeed techsupport team
Bill