If your led matrix doesn’t match the rainbowduino pinout then you are going to have to remap the pins from the matrix to the rainbowduino, or do it in software. Looking at the pin mappings on 2 different 8x8 RGB matrix units it’d would be no mean feat to do it in software so you could plug them directly into a rainbowduino, it would likely be quite impractical to do it in software too.
Heres a short rundown of how I remapped my 8x8 matrix to the rainbowduino.
The rainbowduino expects red and blue pins on one side in 2 blocks of 8 pins, on the other side it wants anode and green pins, 4 anodes, 8 green, 4 anodes.
If you posted the datasheet for your 8x8 matrix it would make things a lot easier. I’ll describe roughly how to translate the pin mappings from my datasheet and you can apply it to yours.
write out 2 columns, 1-16 in the first column and 17-32 in the 2nd. these will be the pins on the LED matrix.
1 17
2 18
3 19
. .
. .
16 32
The led matrix diagram will have 8 rows down the side(should be numbered 1-8), each having a pin number next to it.
it will also have 8 columns, each with a group of 3 pins (each number representing a colour, there will be a key as to which led diagram is which colour). We are going to translate the Row and columns to the anode/colour pins.
so, find Pin 1 in the matrix diagram and write down what it is in the list, here is the mapping on my matrix:
01 = column 1 Red LED 17 = Column 8 Blue LED
02 = Column 1 Green LED 18 = Column 8 Red LED
03 = Column 2 Blue LED 19 = Column 7 Green LED
04 = Column 3 Red LED 20 = Column 6 Blue LED
05 = Column 3 Green LED 21 = Column 6 Red LED
06 = Column 4 Blue LED 22 = Column 5 Green LED
07 = Row 8 Anode 23 = Row 4 Anode
08 = Row 7 Anode 24 = Row 3 Anode
09 = Row 6 Anode 25 = Row 2 Anode
10 = Row 5 Anode 26 = Row 1 Anode
11 = Column 5 Red LED 27 = Column 4 Green LED
12 = Column 5 Blue LED 28 = Column 4 Red LED
13 = Column 6 Green LED 29 = Column 3 Blue LED
14 = Column 7 Red LED 30 = Column 2 Green LED
15 = Column 7 Blue LED 31 = Column 2 Red LED
16 = Column 8 Green LED 32 = Column 1 Blue LED
once you have them all listed you can now start to map them out to the pins on the rainbowduino in groups of 8, here is the blue set of rainbowduino pins and the pins they should connect to on my matrix.
blue matrix
pin 1 pin 32
pin 2 pin 03
pin 3 pin 29
pin 4 pin 06
pin 5 pin 12
pin 6 pin 20
pin 7 pin 15
pin 8 pin 17
Repeat for Red, Green and Anode connections on the rainbowduino.
I hope that helps a bit 
regards,
Reggie.