DC Split Core Current Transformer - for 0-2A

Hi

I have an application - were I need to measure the current (by non-invasive means) of a beacon light
for a safety system.

The current will vary between 0-2A DC (24VDC supply)

I need to use a 0-5VDC ADC input

Do you have a suitable Split Core current transformer for this task: similar to:
seeedstudio.com/depot/noninv … th=144_154

Many Thanks

Ian

Dear customer,

Sorry, for now we just only sell AC current sensor(by non-invasive means).

But if you need find a DC current sensor it is should be invasive.
Because DC current should string with device together then can measurement.

Best regards,

Yuri