Hello,
I’m wondering if there are any data sheets available for the components in the sidekick kit.
Specifically I’m looking for a data sheet for the included buzzer for the rated frequency/voltage/current.
Thank you!
Hi there, please refer to <LINK_TEXT text=“http://wiki.seeedstudio.com/Sidekick_Ba … rduino_V2/”>http://wiki.seeedstudio.com/Sidekick_Basic_Kit_for_Arduino_V2/</LINK_TEXT>. 
Here is the spec for buzzer.
1 Rated Voltage (VDC) 3
2 Operating Voltage (VDC) 1.5~5
3 Resonant Frequency (Hz) 2700±300
4 Sound Output at 10cm (dB) ≥85
5 Current Consumption (mA) ≤30
6 Operating Temperature (℃) -20~+70
7 Storage Temperature (℃) -30~+80 
Seeed techsupport team
Bill