Got the danger shield and in the process of assembly, i noticed that i did not have any 680Ω resistors, i only had 560Ω but i had enough 560Ω to account for the 680Ωs that i didn’t have, so could i use the 560Ωs in replacement of the 680Ωs?
I believe the 680Ωs are for the 7-segment display so maybe its just a different spec than the one on the wiki? the presented information on the product page is the same as the info from the wiki so i didnt know if seeedstudio just used different parts when assembling it.