correct type of the JST-Connector

Hi,

I’m looking for an accu for my rephone. Can anyone explain the correct type of the JST-connector?
(See JST_connector on Wikipedia)

I think, it should be a “JST-SH 2Pin” like on this page: micronwings-com HintsAndTips/RCConnecorTypes/JSTSH2P
(please replace the “-” with proper “/” and “.” the forum here ist very restrictive in writing urls)

Thanks!

Yes, I think this is JST 1.0 (1mm pitch) connector.
You can see it in the eagle files of the Xadow GSM+BLE.

Regards,
Roberto.

Thank you, I’ve got the right connector now.
These type seems not to bey very common. There was exactly one seller on ebay germany …