Should be possible if you are willing to live without the GPS? I’m curious if anyone has tried it as well. The CPU and Lora are the same, so seems you could run it as a meshtastic communicator, but it would not support tracking except with the phone GPS. (T1000-E has an additional added GPS receiver that doesn’t require the online computation used by the LR1110 GPS solution.)
2 Likes