Hi
I have just purchased a Respeaker 4 Mic Array for the Raspberry PI (Mine is Model 3B+) and i have installed the drivers and got the microphones working correctly. I then when on to install the Alexa for Raspberry PI (https://github.com/alexa/avs-device-sdk/wiki/Raspberry-Pi-Quick-Start-Guide-with-Script) which works well with the ReSpeaker 4Mic array.
I now want to extend the Alexa App which is written in C++ to control the LED’s on the ReSpeaker. I have run the python examples and the Raspberry PI can control the LEDs as expected.
I understand that the LED’s are controlled via the SPI interface. Do you have any example code in C++ to control the LED’s or any resources to do this.
Many thanks.
Peter Tewkesbury
Hello,
I’ve got exactly the same problem.
I would like to use led in C++ from Respeaker 4 Mic Array but I don’t find any samples.
I need help too.
Regards,
What about that one:
https://github.com/snipsco/snips-skill-respeaker
Hi there,
- You have to turn on the spi first.
sudo raspi-config
Go to “Interfacing Options”
Go to “SPI”
Enable SPI
Exit the tool
- use
gpio -v to verify if you install wiringpi library correctly.
http://wiringpi.com/download-and-install/
- then you can create led.cpp file. you can understand the apa102 logic by reading
<LINK_TEXT text=“https://cpldcpu.wordpress.com/2014/11/3 … -superled/”>https://cpldcpu.wordpress.com/2014/11/30/understanding-the-apa102-superled/</LINK_TEXT>
[code]#include <wiringPi.h>
#include <wiringPiSPI.h>
#include
#include <stdint.h>
int main() {
wiringPiSetup();
if(wiringPiSPISetup(0, 6000000) < 0) {
std::cerr << “wiringPiSPISetup failed” << std::endl;
}
pinMode (21, OUTPUT);
digitalWrite (21, HIGH);
uint8_t buf[1];
for(int i = 0; i < 4; i++) {
buf[0] = 0x00;
wiringPiSPIDataRW(0, buf, 1);
}
uint8_t r, g, b, brightness;
r = 0xFF;
g = 0x00;
b = 0x00;
brightness = 100;
uint8_t led_frame[4];
for(int i = 0; i < 12; i++) {
led_frame[0] = 0b11100000 | (0b00011111 & brightness);
led_frame[1] = b;
led_frame[2] = g;
led_frame[3] = r;
wiringPiSPIDataRW(0, led_frame, 4);
}
for(int i = 0; i < 4; i++) {
buf[0] = 0xFF;
wiringPiSPIDataRW(0, buf, 1);
}
delay(5000);
return 0;
}
[/code]
4. run below command to compile the file
g++ -Wall -o led led.cpp -lwiringPi
5. run below command
sudo ./led
thanks.