Hello,
I request your help to connect my rpi 4 to my serial camera Grove-Serial_Camera with groovepi
i try to connect my camera to the RPISER port and the SERIAL port but the result is the same : i was unable to receive anything from the camera
i try multiple connections but all failed :
- with python
import serial
try:
serialPort = serial.Serial("/dev/ttyAMA0", 9600, timeout = 2)
print “Port opened, with sync”
bytes_sent = serialPort.write(“AA0D00000000”)
print "bytes sent : ", bytes_sent
while True:
line = serialPort.read(6)
print line
serialPort.close()
except IOError as e:
print "Error ", e
the result : no data received :
"
pi@dex:~/prg/MyRobot $ sudo python test.py
Port opened, with sync
bytes sent : 12
"
I send “sync” command according to camera protocol but i never received “ack”
i try to disconnect the camera from the rpiser port and connect instead a gps grove module that i have on the same port and i receive data :
"
pi@dex:~/prg/MyRobot $ sudo python test.py
Port opened, with sync
790,
M,M$G
PGGA,0
00*79
"
So i think the issue is not grove and not rpi configuration, but i think the command that i send was never received or is incorrect
i try also in java and with “cu” command without sucess
If someone have an idea to help me etablish connection with my camera, it will be great ![]()