Hi Folks,
I would like to plug an haptic motor (3.7V - 38mA) to the XIAO Expansion board through the A0-D0 grove.
This is the schematic of the A0-D0 grove of the expansion board:
Just for information, this is the link to the full schematic:
Does that mean I just need to remove the 2nd and 3rd wire of my grove connector?
That would look like this:
and connect the 2 wires to the haptic motor ?
I did not see many applications that need only 1 positive wire and ground.
Most of the applications I saw use a remote control and a grove IC.
So I just wanted to see if it was right.
Would appreciate any input.
Thank you.
Cheers!