Now I have Wio terminal. I bought ReSpeaker-2Mics for RPI last year.
Does ReSpeaker-2Mics work on Wio Terminal?
Where can I get a driver on Wio Terminal?
Hi @yoshy, I think from the wiki page, it’s mentioned that ReSpeaker 2-Mics Pi HAT only supported following platforms, not the WIO Terminal at the moment.
- Raspberry Pi (Support Raspberry Pi Zero and Zero W, Raspberry Pi B+, Raspberry Pi 2 B, Raspberry Pi 3 B, Raspberry Pi 3 B+, Raspberry Pi 3 A+ and Raspberry Pi 4)
- NPi i.MX6ULL Dev Board Linux SBC
- ODYSSEY – STM32MP157C
- Nvidia Jetson Nano Series.
OK.
Then I should write down Python code or other Lang. code to control mics, speaker over I2S in Wio.
Thanks,