Hello world,
I have a circular 4-mic respeaker array on which there are two Grove ports available.
I also have two Grove sensors
- an ultrasonic ranger
- sound detection
I was hoping to be able to plug at least one of them into one of Respeaker Grove sockets and make them operational, however, without success.
What library should I use ?
Any piece of information would be helpful.
D.
Hi,
For grove-ultrasonic sensor, please plug into gpio12, NOT I2C. then follow below instructions.
pi@raspberrypi:~ $ git clone https://github.com/Seeed-Studio/grove.py.git
pi@raspberrypi:~ $ cd grove.py/
pi@raspberrypi:~/grove.py $ sudo python setup.py install
pi@raspberrypi:~/grove.py $ cd grove
pi@raspberrypi:~/grove.py/grove $ python grove_ultrasonic_ranger.py 12
Detecting distance…
223.759947152 cm
142.985376818 cm
223.776389813 cm
5.44663133292 cm
9.18733662572 cm
16.5700912476 cm
Warning: the distance from the ultrasonic ranger is not accurate
26.7234341852 cm
223.31188465 cm
223.792832473 cm
11.107017254 cm
Bill
anenin
3
Hi!
I have similar problem but with Grove - PIR Motion Sensor. I’ve followed the instructions above, but instead of the last tep, I did:
python grove_mini_pir_motion_sensor.py 12
the result is nothing - no error, no return of any values. I’m also not sure that mini pir is correct choice since i have a regular pir motion sensor.
UPDATE: when I run ultrasonic ranger - I start to receive some output, with worning that it is incorrect. (Obviously, since I plugged motion sensor).
Best regards,
Andrei
bill.yu
4
Hi there,
I tested the min pir and pir with connection to GPIO 12. both of them work. For more info, please refer to instruction from <LINK_TEXT text=“https://github.com/Seeed-Studio/grove.p … /README.md”>https://github.com/Seeed-Studio/grove.py/blob/master/README.md</LINK_TEXT>
pi@raspberrypi:~ $ grove_mini_pir_motion_sensor 12
Motion detected.
Motion detected.
Motion detected.
Motion detected.
Motion detected.
Motion detected.
Motion detected.
Motion detected.
thanks
Bill