At the moment I do not have a Seeduino or similar board. I only have access to Arduino uno, mega and nano. I would like to connect the 9 DOF imu to one of these boards. I have downloaded the Zip library from github (from this tutorial - Grove - IMU 9DOF v2.0 | Seeed Studio Wiki)
I use the sample code IMU_9DOF_Demo_Compass_Calibrated. I have not done any changes to the file. I connected the IMU to SCL, SDA, 5V and GND - I tested both on the mega and the uno.
I am also getting a āConnection Failedā message, but I am using a Seeduino Lotus board. I have run I2C Scanner and the address is 0x69 and Iāve tried changing the address, and still no joy.
Happy to create a new thread instead of hijacking this one, but thought Iād just jump in as Iām having similar issuesā¦