Hi Folks, I want to make a mini-player which presents a USB interface which connects a file system (ie., the SD card on either the Music Shield or the USBDroid) in a straightforward way such that, for example, a car stereo with USB memory stick support will be able to read the music off it to playback AND is capable of pairing with a (specific, predefined and prenamed) Bluetooth headset and streaming Audio to the headset.
I think I will need to add an LCD module to my list, of course I will be adding buttons too.
Please forgive me if obvious answers to my following questions are within search/click range of me here - I’ve done some searching and reading but found nothing to make me very sure either way.
Does anybody know as a certainty that it is possible using the Music Shield ( seeedstudio.com/depot/blueto … th=132_134 ) ?
(Alternatively: Is anybody convinced that streaming audio via Bluetooth is unlikely due limitations of either the Music Shield or Bluetooth Shield ?)
Can/would anybody advise a different choice for the base of this project than the USBDroid ?