Code in arduino IDE for Brushed motor connected with Mini Motor driver V1

Thank you for responding, PJ. The code I’m trying to compile (below) is the example code from the repo seedstudio…/Grove-Mini_I2C_Motor_Driver_v1.0. I did not write it. BTW, this is the repo recommended on the wiki page.

The photo above is from the original poster, not me. I’m simply trying to compile the example code with the XIAO_ESP32S3 board selected in the Arduino IDE. I don’t even have the motor driver board connected at this point.

Here’s the code:

/****************************************************************
    Example code demonstrating the use of the Arduino Library for
    the SparkFun MiniMoto board, which uses the TI DRV8830 IC for I2C
    low-voltage DC motor control.

    This code is beerware; if you use it, please buy me (or any other
    SparkFun employee) a cold beverage next time you run into one of
    us at the local.

    17 Sep 2013- Mike Hord, SparkFun Electronics

    Code developed in Arduino 1.0.5, on a Fio classic board.

**Updated for Arduino 1.6.4 5/2015**
****************************************************************/

#include <SparkFunMiniMoto.h>  // Include the MiniMoto library

// Create two MiniMoto instances, with different address settings.
MiniMoto motor0(0xC4); // A1 = 1, A0 = clear
MiniMoto motor1(0xC0); // A1 = 1, A0 = 1 (default)

#define FAULTn  1     // Pin used for fault detection.

// Nothing terribly special in the setup() function- prep the
//  serial port, print a little greeting, and set up our fault
//  pin as an input.
void setup() {
    Serial.begin(9600);
    Serial.println("Hello, world!");
    pinMode(FAULTn, INPUT);
}

// The loop() function just spins the motors one way, then the
//  other, while constantly monitoring for any fault conditions
//  to occur. If a fault does occur, it will be reported over
//  the serial port, and then operation continues.
void loop() {
    Serial.println("Forward!");
    motor0.drive(100);
    motor1.drive(100);
    delayUntil(1000);
    Serial.println("Stop!");
    motor0.stop();
    motor1.stop();
    delay(1000);
    Serial.println("Reverse!");
    motor0.drive(-100);
    motor1.drive(-100);
    delayUntil(1000);
    Serial.println("Brake!");
    motor0.brake();
    motor1.brake();
    delay(1000);
}

// delayUntil() is a little function to run the motor either for
//  a designated time OR until a fault occurs. Note that this is
//  a very simple demonstration; ideally, an interrupt would be
//  used to service faults rather than blocking the application
//  during motion and polling for faults.
void delayUntil(unsigned long elapsedTime) {
    // See the "BlinkWithoutDelay" example for more details on how
    //  and why this loop works the way it does.
    unsigned long startTime = millis();
    while (startTime + elapsedTime > millis()) {
        // If FAULTn goes low, a fault condition *may* exist. To be
        //  sure, we'll need to check the FAULT bit.
        if (digitalRead(FAULTn) == LOW) {
            // We're going to check both motors; the logic is the same
            //  for each...
            byte result = motor0.getFault();
            // If result masked by FAULT is non-zero, we've got a fault
            //  condition, and we should report it.
            if (result & FAULT) {
                Serial.print("Motor 0 fault: ");
                if (result & OCP) {
                    Serial.println("Chip overcurrent!");
                }
                if (result & ILIMIT) {
                    Serial.println("Load current limit!");
                }
                if (result & UVLO) {
                    Serial.println("Undervoltage!");
                }
                if (result & OTS) {
                    Serial.println("Over temp!");
                }
                break; // We want to break out of the motion immediately,
                //  so we can stop motion in response to our fault.
            }
            result = motor1.getFault();
            if (result & FAULT) {
                Serial.print("Motor 1 fault: ");
                if (result & OCP) {
                    Serial.println("Chip overcurrent!");
                }
                if (result & ILIMIT) {
                    Serial.println("Load current limit!");
                }
                if (result & UVLO) {
                    Serial.println("Undervoltage!");
                }
                if (result & OTS) {
                    Serial.println("Over temp!");
                }
                break;
            }
        }
    }
}