Hello,
is it possible that anyone from Seeedstudio checks my example
production files?
It is only an example board with slot hole pad (Pad2) and an
board cutout.
I only want to know if this example files are OK for production.
Tanks for any reply.
Martin
example_board_gerbers.zip (12.6 KB)
            
 
            
              
              
              
            
           
          
            
            
              no problem, we can do that
             
            
              
              
              
            
           
          
            
            
              Hi, I also want to order the attached through your fusion service.
My pcb has a AXT526124 (0.4 mm pitch) socket for a e-paper display. I created the footprint myself and verified it.
It is a simple breakout board.
Can somebody verify that the generated files are correct ? The Gerber output was generated using ARES (Proteus)
I would be grateful!
chinedisp-2 breakout - CADCAM.ZIP (5.75 KB)
            
 
            
              
              
              
            
           
          
            
            
              hi there,
i have checked your gerber files, everything is ok