Card Tracker T1000-E as a tracker?

Hey folks!
Now I can confirm that the T1000E has a Flash Chip of 8192 KB. The trick is to set pin 45 high to enable the flash chip. Maybe it is also necessary to change #define PIN_QSPI_IO3 to (32) instead of (33). See pinout

/wiki.openelab.io/seeed-studio/sensecap-card-tracker#get-started

Until now I have no clue what this flash contains.

2 Likes