Capture signal from IC

I want measure the Dout word so I can use it in a PIC application, but I need to know what’s sent!
Connected to RF, it’s a remote control for home electrical appliance (Everflourish).

OK, I tried the settings but not all of the signal was captured, it was truncated.

I tried the setting Post Trigger function under “Buff Pri” but there seems to be a bug here, almost all (2/3) buffer capacity is before trigger instead of after the trigger as it should be.

Suggestion, in “SING” trigger, put all available buffer capacity after trigger, nothing interesting will happen before.

Thanks for helping me.