Can't upload the BOM file

Hello,



I created a BOM file following the example at https://www.seeedstudio.com/fusion_pcb.html. However i get the error
</s>We can't read the BOM file, please modify the format according to the BOM File Guideline. Error: The quantity must be an integer value.<e>

This is my BOM file:
</s><i> </i>Designator,Manufacturer Part Number,Quantity C1,C2,CC0402JRNPO9BN180,2 C4,CC0402KRX7R8BB104,1 CN1,CN2,CN3,F185-1108A1BSYC1,3 D1,CX-G302DC,1 D3,SR302DC,1 D4,B5819W,1 J1,J2,J3,J5,F185-1104A1BSYA1,4 R2,RC0402JR-0710KL,1 R3,R4,RC0402JR-07100KL,2 R5,RC0402JR-07910KR,1 R6,R7,RC0603JR-07560KL,2 R8,RC0402JR-07910KR,1 SW1,TS-1101F,1 U1,ATMEGA328P-AU,1 <e>

What am I doing wrong?



Kind regards,



Chris
BOM.xlsx (9.84 KB)

Hi Chris,



When I opened the files in Excel the data is not separated into columns and there are only commas separating each value. So the system is reading your data as Designator = C1, MPN = C2 then Quantity = CC0402JRNPO9BN180. Just check out out the template to see how to organise the data.