I have been having a bunch of problems installing Linux OSs to the Odyssey. The first issue I encountered was that installs would go completely fine, but upon restarting, it appeared no bootloader was written, as the windows bootloader still remained. So I loaded up Gparted and wiped the partition table on the MMC storage completely scrubbing the included windows install, and then fired up a Linux Mint live usb to try installing Mint to the MMC again. Now Mint won’t even fully install - partitioning seems to work but during writing system files it always stops saying the media is faulty.
I have booted GParted and tried running badblocks/e2fsck on the MMC but no issues are found. I have also tried installing another distro, Void Linux, but it too can’t successfully install. I have tried multiple USB/microSD cards for the installers and the self-validation test doesn’t find any corruption on the installer drives I am using.
I have also tried all of the relevant BIOS options, including turning on CSM with UEFI and with Legacy mode, no change.
The closest I got to possibly fixing this was that the ubuntu package “boot-repair” claimed SecureBoot was enabled and so it could not perform repairs - but the BIOS has no SecureBoot setting whatsoever (VERY odd! Virtually every x86 computer I’ve used has had this), and CSM did not affect this error.
Any idea why I can’t seem to successfully repartition & install a linux OS to the built in storage?