Can't connect to XIAO nrf52840 SWD interface

I bought a XIAO expansion board to be able to more easily program the XIAO nrf52840 through SWD. I’m using SEGGER J-Link Mini Edu debugger. I connect the GND, SWDCLK and SWDIO pins from my debugger to the corresponding pins on expansion board. However, after all this, the device still doesn’t show up (I tried with nordic vscode extension and segger flash program). I turned the board on. I tried with and without powering from usb. I tried connecting the J-link VCC to the 3.3V pin on the expansion board. I tried holding the XIAO down as well as with soldered pins. But it seems whatever I do, my computer won’t detect the device… PS: i noticed the expansion’s board “on” light doesn’t light up…

What am I doing wrong?

I also noticed that the area below the XIAO on the expansion board becomes very hot after a few seconds. Not sure if this is normal.

If J-Link has an input pin like VoltageTarget, try connecting it to the 3V3 pin of XIAO.
J-Link should need to know the voltage of the target device.

There is no power exchange between J-Link and XIAO. The reason it is getting hot is because it is connected incorrectly.

Which part is connected incorrectly? When I just connect the XIAO nrf52840 to usb, it doesn’t get hot (without expansion board). It starts getting hot only after connecting it to the expansion board. I am starting to worry there is a defect in my expansion board.

The first board I got also got hot; I had to have it replaced because the USB current consumption was about 300mA.

Is it the XIAO that gets hot or the expansion board? In my case, it was the IC on the expansion board side, located directly below the XIAO.
Will Blink.ino for example work properly if XIAO is not attached to the expansion board?

I have the same problem but I just connect all of the pins. i didn’t work at all.
J-Link Command File read successfully.

Processing script file…

J-Link connection not established yet but required for command.

Connecting to J-Link via USB…O.K.

Hardware version: V9.70

VTref=3.269V

Selecting SWD as current target interface.

Selecting 400 kHz as target interface speed

Device “NRF52840_XXAA” selected.

Connecting to target via SWD

InitTarget() start

InitTarget() end - Took 110ms

InitTarget() start

InitTarget() end - Took 111ms

Error occurred: Could not connect to the target device.

Script processing completed.

Hi there,

And Welcome here…

So , can you show a picture of this apparatus,
From the Log it’s got a bad connection. Start there.
also Slow it down use 100khz , also which JLink device you using?

Your close , keep at it.

HTH
GL :slight_smile: PJ :v:

Here is my AI summery Document, Thank you sir!

# J-Link SWD Debug Session Report — XIAO nRF52840 (Sense)

**Date:** 2026-09-09/10 (CST)

**Probe:** SEGGER J-Link V9 (HW V9.70, FW compiled 2021-05-07), S/N 20781318

**Target:** Seeed XIAO nRF52840 (Sense), combo firmware (S140 SoftDevice @ 0x0 + Adafruit UF2 bootloader @ top of flash)

**Host:** macOS (J-Link SWD software V9.34b installed via cask)

**Goal:** Verify whether the J-Link probe can connect to the nRF52840 over SWD.

—

## 1. Executive Summary

**The J-Link probe, host software, cabling, and target power are all verified healthy. The target’s SWD debug port does not respond at the physical (DP) layer — no ACK is ever returned for the DP IDCODE read, across four independent software stacks and four clock speeds. All software-side causes are ruled out. The failure is electrical: the chip either has its debug port locked (APPROTECT) or its SWD front-end / the board’s SWD path is defective. The two remaining discriminators are a known-good target board and/or a known-good probe.**

—

## 2. Hardware Setup

| Item | Detail |

|—|—|

| Probe | SEGGER J-Link V9, HW V9.70, FW 2021-05-07, S/N 20781318 |

| Probe connector | 9-pin SWD (1=VTref, 2=SWDIO, 3=GND, 4=SWCLK, 9=nRESET) |

| Target wiring | XIAO SWDIO → J-Link TMS/DIO; XIAO SWCLK → J-Link TCK/CLK |

| Ground | Common ground wired between probe and board |

| Target power | USB from host (3.3 V rail sensed: VTref = 3.25–3.27 V) |

| nRESET | Initially **not connected**; connected later (J-Link reports it cannot drive it low — see §5) |

| Board history | This XIAO has **never** been connected via SWD; all previous flashing was USB DFU / UF2 drag-drop |

—

## 3. Software Stacks Used (all independent)

1. **SEGGER J-Link Commander** (`JLinkExe` V9.34b) — proprietary SEGGER DLL

2. **probe-rs** 0.32 (CLI `probe-rs info`) — open-source, own J-Link protocol implementation

3. **Nordic nrfjprog** 9.4.0 (from Seeeduino Arduino package) — Nordic DLL

4. **nRF Connect for Desktop** (Programmer app, nrfutil stack) — Nordic’s current toolchain

5. (Attempted) Nordic nrfjprog 9.4.0 + **SEGGER libjlinkarm V9.34.2 dylib** via `–jdll`

—

## 4. Test Results Timeline

### 4.1 J-Link / probe identification

- macOS USB enumeration: probe found by both `probe-rs list` and SEGGER software.

- `nrfjprog --ids` → `20781318`. **Probe itself is fully functional.**

### 4.2 SWD connect attempts — JLinkExe

Script used (`swd_test.jlink`):

```

si SWD

speed 400

device nRF52840_xxAA

connect

exit

```

Result (identical at 100 kHz, 400 kHz, 1 MHz, 4 MHz):

```

Connecting to J-Link via USB…O.K.

VTref=3.267V

Selecting SWD as current target interface.

Device “NRF52840_XXAA” selected.

Connecting to target via SWD

InitTarget() start

InitTarget() end - Took 110ms

InitTarget() start

InitTarget() end - Took 111ms

Error occurred: Could not connect to the target device.

```

- No `Found SWD-DP with ID 0x2BA01477` line ever appears → **DP IDCODE never read successfully**.

- Generic `Cortex-M4` device also fails identically (rules out device-description issues).

### 4.3 probe-rs verbose (RUST_LOG=debug)

```

Performing SWD line reset

Reading DPIDR to enable SWD interface

Transfer 1/1 failed: Failed(NoAcknowledge)

```

Repeated ~10×. → The probe issues the SWD line reset and DPIDR read correctly; **the target never pulls SWDIO low to ACK** — no response at the very bottom of the SWD protocol.

### 4.4 Nordic nrfjprog

```

nrfjprog --memrd 0x10000000 --n 8

ERROR: Cannot connect to any nRF device.

```

Same failure as above.

### 4.5 nRF Connect for Desktop (Programmer)

```

Reading readback protection status for Application core

Failed … Device error: Setting the debug port SELECT register failed while

powering up sys and debug regions (Unknown error in the J-Link DLL (error code =-1)).

This might indicate that the debug port is unavailable. Double-check device

power supply and SWD lines, and ensure that SWD is not disabled

```

Note: the tool cannot even complete the debug-domain power-up handshake — consistent with a debug port that is either unpowered/unresponsive at the DP level or actively refused.

### 4.6 Recover / Erase attempts

```

nrfjprog --recover --family NRF52 --snr 20781318

Recovering device. This operation might take 30s.

ERROR: Recover failed.

```

- Also retried with the latest SEGGER dylib (`–jdll /Applications/SEGGER/JLink_V934b/libjlinkarm.dylib`) — same failure.

- nRF Connect “Erase all” also fails at the same step (protection-status read / debug-power-up).

- **Interpretation:** recover still requires an initial SWD DP connection (CTRL-AP is reached *through* the DP). Since the DP never ACKs, recover cannot proceed. Recover failure therefore does **not** prove APPROTECT — it only confirms the DP layer is unreachable.

—

## 5. Multimeter / Electrical Verification

All measurements taken with the target powered from USB.

| Measurement | Result | Meaning |

|—|—|—|

| VTref (J-Link senses target 3.3 V) | 3.25–3.27 V | Target power rail present; power wiring OK |

| Continuity J-Link pin ↔ XIAO pad (each line) | ~3 Ω, stable | Cables/solder joints electrically continuous |

| Wire-swap test (SWDIO/SWCLK swapped) | Still no connect | Not a swapped-wire issue |

| Re-soldering the connections | Still no connect | Not a cold-joint issue |

| SWDIO pad ↔ GND (**J-Link disconnected**, powered) | ~3 V | Chip internal pull-up active → pad truly reaches the chip’s SWDIO pin |

| SWCLK pad ↔ GND (**J-Link disconnected**, powered) | ~0 V | Chip internal pull-down active → pad truly reaches the chip’s SWCLK pin |

| SWCLK pad during connect attempt | **Voltage toggling** | J-Link clock signal does arrive at the pad |

| SWDIO pad during connect attempt | Only 3.3 → 3.1 V micro-dither | NOT a real 0–3.3 V data swing — looks like crosstalk, not an ACK |

| nRESET (after connecting pin 9 → RST) | J-Link warning: `RESET (pin 15) high, but should be low` | J-Link cannot pull the reset line low — nRESET does not reach the chip’s reset network either |

**Key conclusions from electrical tests:**

- SWDIO/SWCLK pads are the genuine debug pins (internal pull-up/pull-down states match nRF52 default debug-port behavior) and are connected to a live chip.

- The chip is alive: it enumerates on USB (visible as a second device in nRF Connect) — so the MCU core runs, ruling out System OFF / dead chip as the cause of zero SWD response.

- Clock reaches the pad, yet the chip never ACKs → the debug port is refusing or unable to respond.

—

## 6. Ruled Out vs. Remaining Hypotheses

### Ruled out (evidence-backed)

| Hypothesis | Why ruled out |

|—|—|

| Probe broken / not enumerated | Probe listed by SEGGER, probe-rs, nrfjprog; FW up to date (Configurator) |

| Host driver / software bug | 4 independent stacks, 3 different vendors, identical failure |

| Clock speed | 100 kHz–4 MHz all fail identically |

| Target not powered | VTref 3.27 V; USB enumeration works; SWDIO internal pull-up alive |

| Missing / wrong ground | GND wired; stable VTref reading |

| Swapped SWDIO/SWCLK | Swap test failed identically |

| Cold solder joints / broken wires | ~3 Ω continuity; re-soldering changed nothing |

| Pads not connected to chip | SWDIO=3 V (pull-up), SWCLK=0 V (pull-down) prove chip-side connection |

| Firmware re-purposing SWD pins | nRF52840 SWDIO/SWCLK are dedicated debug pins (QFN48 pin 26/27), not GPIO-muxed — firmware cannot steal them |

| Chip in System OFF / deep sleep | USB enumerates — core is running |

| J-Link firmware outdated | Configurator: “firmware already up to date” |

### Remaining hypotheses

1. **APPROTECT (read-back protection) enabled** — would explain a silent debug port; but the “IDCODE not even readable” symptom is atypical (APPROTECT usually still permits DP IDCODE reads), so this is **not confirmed**.

2. **Defective SWD front-end on the chip** (silicon or internal bond issue) while the rest of the chip runs fine.

3. **Board-level fault between the labelled pads and the chip’s actual SWD pins** that still passes static pull-up/pull-down checks but fails under driven signals (less likely given the pad measurements).

4. **Defective SWD output stage on the probe** (VTref sensing works, but the SWDIO/SWCLK line drivers may be dead) — cannot be confirmed without a second target.

—

## 7. Remaining Discriminating Tests (next steps)

1. **Known-good target board** — connect this J-Link to a second XIAO (or any SWD-capable Cortex-M board):

- Connects → J-Link is fine; this specific XIAO has a locked/defective debug port → treat as SWD-dead, keep using USB DFU, or replace board.

- Also fails → the J-Link’s SWD line drivers are defective → replace/repair the probe.

2. **Known-good probe** — if a second J-Link / DAPLink / ST-Link is available, try it on this XIAO to confirm the target side.

3. If a fresh XIAO connects fine: **immediately verify SWD before flashing**, then flash the combo firmware (S140 + bootloader) and confirm the debug port stays reachable — establishing a clean baseline for future SWD work.

—

## 8. Test Scripts

The two scripts below reproduce the entire SWD connection test. Both live in the repository `tools/` directory (same folder as this report).

### `swd_test.jlink` — J-Link Commander script

```text

si SWD

speed 400

device nRF52840_xxAA

connect

exit

```

| Line | Purpose |

|—|—|

| `si SWD` | Select Serial Wire Debug as the target interface (nRF52840 has no JTAG) |

| `speed 400` | SWD clock = 400 kHz (also tested at 100 kHz / 1 MHz / 4 MHz — identical result) |

| `device nRF52840_xxAA` | Target device description loaded by J-Link |

| `connect` | Establish the SWD connection (performs line reset → reads DPIDR → fails with no ACK) |

| `exit` | Quit |

### `run_test.sh` — one-shot wrapper

```bash

#!/bin/bash

# XIAO nRF52840 SWD 连接测试 —— SEGGER J-Link

# 用法: ./run_test.sh [SN]

# 成功标志: 输出含 “Found SWD-DP with ID 0x2BA01477” + “Cortex-M4 identified”

# 失败标志: “Could not connect to the target device” (NoAcknowledge)

SN=“${1:-000020781318}”

JLinkExe -SelectEmuBySN “$SN” -CommanderScript swd_test.jlink 2>&1 \

| grep -viE “^\s*$|license|compiled|uptime|S/N|^J-Link>”

```

Usage:

```bash

cd ~/Documents/XIAO/tools

./run_test.sh # uses default probe S/N 000020781318

./run_test.sh # explicit probe serial number

```

Pass criteria: output contains `Found SWD-DP with ID 0x2BA01477` and `Cortex-M4 identified`.

Fail criteria: output shows `Could not connect to the target device` (i.e. SWD NoAcknowledge) — the current outcome.

To keep the probe retrying in a loop while measuring pad voltages (see §5):

```bash

while true; do ./run_test.sh; done

```

I use a clamp to keep the XIAO firmly pressed on the pogo pins. Without it, the XIAO regularly failed to program using SWD.

Hi there,

So a couple issues
:face_with_peeking_eye:
you only need 4 Wires BTW, so fix that.
Also You may need to connect under reset if your JLink isn’t official?
What unit is that?
I can appreciate the AI… I can , but man so typical to throw this at it and think its gonna just work, C’mon man…
Can You perform the steps required manually ?
Open Jlink , Connect to the device
Halt it,
Read some registers,
Erase it,
Flash it ,
set it to RUN?

BASIC A,B,C stuff…:grin:
Try that, the AI will work , I have a video on here of CodeX doing this very thing , each step. Generating code, compiling the code, flashing the code and logging the Output.
However the setup required needs to be done or you will get what you have.

from this thread..

Stick with JLink,


or this for Nrf52840..
Start there, can you establish a connection to it? , check your wiring, compare it to what I used on the RAL JLink and connect it the same, I think your mixing too many things together, Stay with the JLink get it working first ,then try different flash methods.

Fix the wires first.
You can Halt, Step, READ registers, Reset the MCU once you get it working , you can do EVERYTHING in Jlink.

HTH
GL :slight_smile: PJ :v:

Get it working then throw the Automation to it :+1: