I recently bought a Gps Air530.
Retrieving NMEA sentences goes fine but when i try to send a command to it, i don’t get any response, not even an error message.
I’ve seen more people struggling with this but i haven’t seen any answer yet.
You are receiveing NEMA output. That means there is nothing wrong with your GPS module and wiring. Since, your GPS is not responding to AT commands, I suggest checking if there is a baud rate mismatch. Also make sure that you are sending the commands in correct format.
By the way, if you ever need proteus libraries for generic GPS modules, you can find here:
I would start with the wire connections, You check the port with loopback wires or any port tests, What is the default baud rate? If you getting good strings back then I would look at the Transmit side of the port and loop it back to be sure it’s coming out, You have software or Hardware flow control enabled?
Xon/Xoff = Software, RTS/CTS or DTR/DSR = Hardware. Or NONE.
can you post a pic of the setup , I’m ordering an Air530 for testing but won’t have it for a few days or a week? So press on
HTH
GL PJ
PJ,
the layout is very simple: just connected the Grove cable from the gps to a Grove board with the Arduino . And in the configuraton of the Arduino, i only see a baud rate. But the cable only has Rx and TX so it must be Xon/Xoff.
I don’t have hardware to connect Serial1 to another computer port to check what comes out. As technician i would like to figure out such things. As customer and simple Arduino user, i would expect that it would not be needed to go into such details
I tried the example of Grove - GPS (Air530) | Seeed Studio Wiki but it doesn’t describe how to configure the thing.
The manual that Seed publishes, basically just the datasheet of the chip, is in Chinese but someone was so kind to translate it: Heltec_AB02S_Mods/Air530 GPS Manual Text English.pdf at master · sivaelid/Heltec_AB02S_Mods · GitHub
And that shows commands like $PGKC243*2A which should return a similar line with the current NMEA lines that are given. I entered that in a minimal sketch(see below) but it doesn’t give any response.
what i forgot to mention: why do i want to send command to the GPS?
the gps sends all its NMEA sentences, over 9600 baud, at a frequency of 1Hz. Every second, it spend 0.7s on sending the data,so i receie positions at a rather low rate and with some delay, i’d like to get it faster.
The chip can do much better than this; to get there, you have to modify some of its settings.
But… i didn’t buy a chip, i bought a Grove board. Maybe the intention of the Grove board is just to demonstrate the basic function of the gps, and, as tepalia02 said, that works. Or maybe there is another reason why on the Grove board, the chip cannot be configured.
On the other hand, the sketch on the wiki contains lines:
if (Serial.available()) // if data is available on hardware serial port ==> data is coming from PC or notebook SoftSerial.write(Serial.read()); // write it to the SoftSerial shield
The example on the wiki uses SoftwareSerial on pin 2,3 instead of the hardware Serial1, don’t now why. Of course I tried exactly that sketch as well but no effect.
Nice, I’ve ordered the last one…so.
Looks like it is connected properly, I would set baud rates the same , just for testing.
The "Grove " is only the connection format and sizes . I’m not a fan because of the proprietary nature of it, Hard to get the connectors and pins. Kind of large also, IMO.
However you can usually find every dongle, sensor or trinklet’ with a grove connector for $$ than most without. but I digress.
So pin 8 sends the NEMA data out to the Arduino at 9600 I see, I get the one second timing.
It is PIN 9 then to send data to it, be sure those white and yellow cable line up.
You send a string with checksum and CR &LF
Ascii or HEX?
OK, so you send it a Query for the Nema data interval First? I think you need to send it the Start or Respond to commands first, but I would test with a terminal and TTL to USB direct first. with something like super terminal. What kind of Arduino is that?
You’ll get it , your close.
HTH
GL PJ
HI, guys.
I received the GPS AIR530 connected it up to the XIAO expansion board’s UART Grove connection. I loaded the code attached and plugged in, After some seconds it started streaming the data to the monitor, Next I fired up the older version of (ver.22.07) U center mentioned in the WIKI and configured it to connect to the Xiao port 21 , Data Started to stream and populate the screens.
I added a Google Maps (Free) API Key to the preferences and It displayed the correct location ON SPOT.
I can send configuration changes no problem with the U center App, Restart the GPS and Everything appears to work fine. Picking up 10 Satellites from inside house at dinning room table next to a window.
The Checksum for the commands MUST be correct for it to accept the cmd.
HTH
GL PJ
/*
GPS pass data Serial test (from serial port tester)
Receives from the main USB serial port, sends to the (Serial 1) port.
Receives from serial port 1(GPS AIR530), sends to the USB main serial (Serial 0).
This example works on Xiao Nref52840 Sense (serial1)port pins 7,8
The circuit:
- GPS AIR530 serial device attached to Serial port 1
- USB Serial Monitor open on Serial port (this one is port 21)
- Once you get data then try the U center app (older version )
- add free Google API key to prefrences to get the whole experiernce. total time 30 minutes
void setup() {
Serial1.begin(9600);
Serial.begin(9600);
while (!Serial);
delay(1000);//relax...Get Ready for serial port
Serial.println();
Serial.println("Power ON \n "); // Let's BEGIN!!
Serial1.print("\r");
}
void loop() {
// read from port 1, send to port 0:
if (Serial1.available()) {
int inByte = Serial1.read();
Serial.write(inByte);
}
// read from port 0, send to port 1:
if (Serial.available()) {
int inByte = Serial.read();
Serial1.write(inByte);
}
}
If you’re having trouble sending commands to a GPS Air530 device, there are a few potential reasons and troubleshooting steps you can try:
1. Check Device Connectivity: Ensure that the GPS Air530 device is properly connected to the power source and any required communication interfaces, such as USB or Bluetooth. Confirm that it is turned on and in a functional state. 2. Verify Command Format: Make sure you are sending the commands in the correct format and syntax as specified in the device’s documentation or programming interface. Double-check for any typos or missing parameters. 3. Communication Protocol: Determine the communication protocol supported by the GPS Air530 device. It might use a standard protocol like NMEA (National Marine Electronics Association) or a proprietary protocol. Ensure that your commands align with the protocol requirements. 4. Confirm Compatibility: Verify that the commands you are attempting to send are supported by the GPS Air530 device. Some devices may have limited command sets or specific requirements for certain functionalities. 5. Test with Different Interfaces: If you are using a specific interface (e.g., USB or Bluetooth) to communicate with the device, try switching to a different interface to see if it resolves the issue. It could be a compatibility or configuration problem with the current interface. 6. Firmware Update: Check if there are any firmware updates available for the GPS Air 530 device. Updating the firmware can address bugs, Rapipay Agent Portal Registration, improve functionality, and ensure compatibility with the command set you are using. 7. Contact Manufacturer Support: If none of the above steps resolve the issue, it may be helpful to reach out to the manufacturer’s customer support for further assistance. They can provide specific troubleshooting guidance or advise on any known issues related to command transmission for the GPS Air530 device.
It’s important to consult the device’s documentation or the manufacturer’s resources for accurate and device-specific instructions.
You need to eliminate the possibilities one by one. First open up the Arduino IDE and serial monitor. No need to run any sketch. Just connect the GPS to your MCU board, set the baud rate and you shall see NMEA messages on the serial monitor. Then you type the commands (try other) in the serial monitor and see if they pass through.
JP, thanks, nice story.
I also got the data properly received and interpreted in U-Center.
But what did you exactly do to send commands to the GPS?
Via the Configuration View, i saw a response to a coldstart command, but with other commands, i didn’t see much happening and most of them i also don’t recognize from the 530 manual. Of course, this gps isn’t a u-blox 5, maybe only some of them work (coincidently?)
When you say that “the checksum must be correct”, it sounds like you entered the commands somewhere manually. Where did you enter them? Do you have an example that worked?